Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the maximum voltage that the RX63N RDK can stand (ext. plug)?

Latest Updated:04/28/2015

Question:

Can any high voltage be applied to the RX63N RDK , due to the presence of an LDO?

Answer:

No, a stable regulated 5.0VDC needs to be applied to this kit, either on the power Jack J4 or the external power header J18.

  • Este artigo foi útil?