Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Supercap purpose on YRDKRL78G14 kit

Latest Updated:06/27/2015

Question:

What is the purpose of the supercap on the RL78G14 RDK designated C72?

Answer:

This supercap preserves the status of the real-time clock inside the WiFi Module, thus allowing the WiFi module to reset quicker and go back to the WiFi network faster.
  • Este artigo foi útil?