Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

HEW Integrated Design Environment

Last Updated: 06/27/2016

Question:

What is High-performance Embedded Workshop (HEW) and how much does it cost?

Answer:

High-performance Embedded Workshop (HEW) is a free GUI-based integrated development environment for the development and debugging of embedded applications for Renesas microcontrollers.

Be advised that there will be no further updates to HEW past v4.09.01 which was released on June 16, 2012. We encourage new designs to migrate to our free e2 studio IDE.

Please refer to the article on migrating projects from HEW to e2 studio if you have concerns.