Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Flash Development Toolkit OS Compatibility

Last Updated: 06/27/2016

Question:

What Operating Systems are compatible with the Flash Download Toolkit? Does the Flash Download Toolkit run in the Linux environment?

Answer:

The Flash Download Toolkit only operates on Windows based machines. Linux is not supported at this time.

Supported Operating Systems:
Windows® 10 (32- and 64-bit versions)
Windows® 8.1 (32- and 64-bit versions)
Windows® 7 (32- and 64-bit versions)

For the most current list & specific details, please refer to: https://www.renesas.com/en-us/products/software-tools/system-requirements.html#prog.