Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Error occurs at build project in e² studio (header file not found).

Latest Updated:04/03/2014

Question:

Error occurs at build project in e² studio (header file not found).

e.g.
../src/sample.c:29:22: fatal error: user.h: No such file or directory

 

Condition:

  • Header file location is defined at "Include file directories" of project property (Check if .cproject file has desired path string)
  • Multi-byte character is included in the header file path string

Answer:

Multi-byte filepath definition is not accepted in eclipse.
Project and sourcecode should be placed at filepath with no Multi-byte characters.

Note:This FAQ is subjected to be applied to Multi-byte OS environment.

Suitable Products
e² studio